Hello All,
I have a beaglebone board.Somedays before I finished debug a simple project with SYSBIOS for just blink a led.It run OK when I debug it in in CCS(with out gel init file already).
But when I try to make a bin file and put to SD card.It can generate a proper bin file but can not boot and run.
my post link command is here:
"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat" "E:\CCS_Workspace\typical_BeagleBone_CortexA\Debug\typical_BeagleBone_CortexA.out" "E:\CCS_Workspace\typical_BeagleBone_CortexA\Debug\typical_BeagleBone_CortexA.bin" "${CG_TOOL_ROOT}/bin/armofd.exe" "${CG_TOOL_ROOT}/bin/armhex.exe" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe" & "C:\ti\AM335X_StarterWare_02_00_00_07\tools\ti_image\tiimage.exe" "0x8000bbd8" "NONE" "E:\CCS_Workspace\typical_BeagleBone_CortexA\Debug\typical_BeagleBone_CortexA.bin" "E:\CCS_Workspace\typical_BeagleBone_CortexA\Debug\typical_BeagleBone_CortexA_ti.bin"
INside the command line I put the entry address from my .map file.It is here:
******************************************************************************
TI ARM Linker PC v5.0.1
******************************************************************************
>> Linked Sat May 11 21:58:23 2013
OUTPUT FILE NAME: <typical_BeagleBone_CortexA.out>
ENTRY POINT SYMBOL: "_c_int00" address: 8000bbd8
Same post link command can work on other sample project in starterware(But without usage of SYSBIOS) on my machine.The only different is the load address is 0x80000000.
I dont know why it can not run with program with SYSBIOS.Could anyone help?
Thank you!