Hi,
My setup is as follows:
- Code composer studio 5.3.0.0009
- DSP/BIOS Version 5.33.06
- CG tools 6.1.17
- EDMA3 LLD version 01.11.03.01
- OMAP-L137 EVM
I try to successfully run the Spi Sample application (in DMA mode) that comes with the pspdrivers_01_30_00_05 package. After modifying some parameters in the code I have successfully run a few SPI instructions, but the subsequent SPI instructions don't work. If the application is modified to first read the flash status register, the first instruction works fine if I use parameters as follows:
spiParams.spiHWCfgData.delay.c2TDelay = 65000u;
spiParams.spiHWCfgData.delay.t2CDelay = 65000u;
dataparam->flags = 0;
My Printf Logs:
EDMA3 : edma3init() passed
write is Enabled
Do you have any tips? Should I adjust any parameters in the code to run the Spi Sample application successfully?
Please help.
Regards,
Stig-Helge Larsen