TI provide a lot of link cmd template, but no any template for this type application. Can anybody provide a template mixing SYS BIOS and CLA- C usage?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI provide a lot of link cmd template, but no any template for this type application. Can anybody provide a template mixing SYS BIOS and CLA- C usage?
I modify TMS320F28069.cmd according to the following .cmd file.
/*==================================================================================*/
/* User specific Linker command file for running from FLASH */
/*==================================================================================*/
/* FILE: F28035_FLASH_HVACI_Sensorless.CMD */
/* */
/* Description: Linker command file for User custom sections targetted to run */
/* from FLASH. */
/* */
/* Target: TMS320F28035 */
/* */
/* Version: 1.00 */
/* */
/*----------------------------------------------------------------------------------*/
/* Copyright Texas Instruments © 2009 */
/*----------------------------------------------------------------------------------*/
/* Revision History: */
/*----------------------------------------------------------------------------------*/
/* Date | Description */
/*----------------------------------------------------------------------------------*/
/* 4/13/09 | Release 1.0 New release. */
/*----------------------------------------------------------------------------------*/
/* Define the memory block start/length for the F28035
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F2803x are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
L0 memory block is mirrored - that is
it can be accessed in high memory or low memory.
For simplicity only one instance is used in this
linker file.
Contiguous SARAM memory blocks or flash sectors can be
be combined if required to create a larger memory block.
*/
MEMORY
{
/* Note that the memory allocation below does not create sections as necessary for
the CLA on the F2803x.
*/
PAGE 0:
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM (L0-L1)*/
RAML3 : origin = 0x009000, length = 0x001000 /* data RAM (L3) */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
BOOTROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 :
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
dataRAM : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */
CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA, PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
Cla1Prog : LOAD = FLASHC, /* Note for running from RAM the load and RUN can be the same */
RUN = RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0, PAGE = 1
.ebss : > RAMM1, PAGE = 1
.esysmem : > RAMM1, PAGE = 1
Cla1Data : > RAML2, PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1
CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
}
SECTIONS
{
/************* DPLIB Sections C28x ************************/
/* ADCDRV_1ch section */
ADCDRV_1ch_Section : > dataRAM PAGE = 1
/* ADCDRV_4ch section */
ADCDRV_4ch_Section : > dataRAM PAGE = 1
/* CNTL_2P2Z section */
CNTL_2P2Z_Section : > dataRAM PAGE = 1
CNTL_2P2Z_InternalData : > dataRAM PAGE = 1
CNTL_2P2Z_Coef : > dataRAM PAGE = 1
/* CNTL_3P3Z section */
CNTL_3P3Z_Section : > dataRAM PAGE = 1
CNTL_3P3Z_InternalData : > dataRAM PAGE = 1
CNTL_3P3Z_Coef : > dataRAM PAGE = 1
/*DLOG_4CH section */
DLOG_4CH_Section : > dataRAM PAGE = 1
DLOG_BUFF : > dataRAM PAGE = 1
/*MATH_EMAVG section */
MATH_EMAVG_Section : > dataRAM PAGE = 1
/*PFC_ICMD section*/
PFC_ICMD_Section : > dataRAM PAGE = 1
/*PFC_INVSQR section*/
PFC_INVSQR_Section : > dataRAM PAGE = 1
/* PWMDRV_1ch driver section */
PWMDRV_1ch_Section : > dataRAM PAGE = 1
/* PWMDRV_1chHiRes driver section */
PWMDRV_1chHiRes_Section : > dataRAM PAGE = 1
/* PWMDRV_PFC2PhiL driver section */
PWMDRV_PFC2PhiL_Section : > dataRAM PAGE = 1
/* PWMDRV_PSFB driver section */
PWMDRV_PSFB_Section : > dataRAM PAGE = 1
/* PWMDRV_DualUpDwnCnt driver section */
PWMDRV_DualUpDwnCnt_Section : > dataRAM PAGE = 1
/* PWMDRV_ComplPairDB driver section */
PWMDRV_ComplPairDB_Section : > dataRAM PAGE = 1
/* ZeroNet_Section */
ZeroNet_Section : > dataRAM PAGE = 1
/************* DPLIB Sections CLA ************************/
/* ADCDRV_1ch_CLA section */
ADCDRV_1ch_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* ADCDRV_4ch_CLA section */
ADCDRV_4ch_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* CNTL_2P2Z_CLA controller sections */
CNTL_2P2Z_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
CNTL_2P2Z_CLA_InternalData : > CLA_CPU_MSGRAM PAGE = 1
CNTL_2P2Z_CLA_Coef : > CPU_CLA_MSGRAM PAGE = 1
/* CNTL_3P3Z_CLA controller sections */
CNTL_3P3Z_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
CNTL_3P3Z_CLA_InternalData : > CLA_CPU_MSGRAM PAGE = 1
CNTL_3P3Z_CLA_Coef : > CPU_CLA_MSGRAM PAGE = 1
/*MATH_EMAVG_CLA sections */
MATH_EMAVG_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
MATH_EMAVG_CLA_InternalData : > CPU_CLA_MSGRAM PAGE = 1
/*PFC_ICMD_CLA sections*/
PFC_ICMD_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
PFC_ICMD_CLA_InternalData : > CPU_CLA_MSGRAM PAGE = 1
/*PFC_INVSQR_CLA sections*/
PFC_INVSQR_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
PFC_INVSQR_CLA_InternalData : > CPU_CLA_MSGRAM PAGE = 1
/* PWMDRV_1ch_CLA driver section */
PWMDRV_1ch_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* PWMDRV_1chHiRes_CLA driver section */
PWMDRV_1chHiRes_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* PWMDRV_PFC2PhiL driver section */
PWMDRV_PFC2PhiL_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* PWMDRV_PSFB_CLA driver section */
PWMDRV_PSFB_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* PWMDRV_DualUpDwnCnt_CLA driver section */
PWMDRV_DualUpDwnCnt_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* PWMDRV_ComplPairDB_CLA driver section */
PWMDRV_ComplPairDB_CLA_Section : > CPU_CLA_MSGRAM PAGE = 1
/* ZeroNetCLA_Section */
ZeroNetCLA_Section : > CPU_CLA_MSGRAM PAGE = 1
}
and there is no error while building. now I want to port iir2p2z demo project to my project.
I see the demo code is based on NO-BIOS, so I have to modify demo code. so anybody had done such work?