Hi, i'm trying to setup and UDP connection with IPv6
While I was using IPv4 I could see the print message of the function NetworkIPAddr (which is called by NC_NetStart ):
"Network Added: xxx.xxx.x.xxx"
But now i'm using an IPV6 address and i can't see that print anymore and the DSP (C6678) cant receive neither send data.
Looking at the source code of NC_NetStart and NetworkIPAddr , I see that both functions require an address in the format IPN (defined in usertype.h). That same header has an type defined por IPv6 which is IP6N, but the compiler gives me an error if I try to cast from one type to another.
How should I proceed in that case? Do I need to rebuild some NDK library for this??
Thanks!