Hi,
I am working on Am335x TI ICE board for the full ethercat project. I am using the example code: protocol/ethercat_slave project.
My configuration: CCS (Version: 5.5.0.00077), am335 SDK (1.1.0.1), bios 6.37.00.20 and xdctools 3.25.03.72.
Yesterday It was Ok to build and debug the application.
Today, I open an other project, I close it and re-open the Ethercat project.
Now, the debogger (at the end of loading) don't find and stop at the entry point (main).If I resume the code, make a hard reset and restart, it's ok.
I have re-installed am 335 SDK 1.1.0.1, same thing...
I have deleted the metadata file in the workspace_v5_5 directory, same thing...
The option <reset the target on connect> is true...
What's going on ?
Where is located the path to help the debuggor to find this entry point ?
Thanks for your reply? Two weeks that I can not find..