Hi,
I am using syslink_2_21_03_11 with OMAP L138. I would like to better understand the way shared region is statically allocated in HLOS. I only understand how to do so on slave processor running SYS/Bios.
AT the following link I found some information http://e2e.ti.com/support/embedded/tirtos/f/355/t/141150.aspx:
"Actually, the method that's the most preferred and the easiest to do, is for you to not call SharedRegion_setEntry dynamically at all. If you want any extra SharedRegion, if you set it statically in the cfg file of the slave (any slave), it gets automatically pulled into and mapped into all processes that may run after that on A8, and you don't need to call SharedRegion_setEntry explicitly on the A8 at all. You can simply call SharedRegion_getHeap and start using the heap for your shared memory allocations. This is the method we suggest as the easiest to use."
How is the map of shared regions passed to other cores? Do I have to allocate at least one shared region on the host too? If so, how do I define the size and the address of the region at the host?
Regards
Gleb