Hi ,
I am trying to activate IPC Late Attach feature with 6AJ.1.3 release. Steps I followed as mentioned in
http://processors.wiki.ti.com/index.php/Early_Boot_and_Late_Attach
Using these tools bios_6_35_04_50, ipc_3_21_00_07, xdctools_3_25_03_72 and arm_5.1.1 to build the example messageq_single xem4. How ever it is mentioned in the link to use bios_6_35_03_47, xdctools_3_25_04_88, TICGTARM_5.0.1,IPC : 3.21.00.07
After loading the xem4 from Single Stage Boot loader getting message from boot loader:
spl_boot_ipu: found resource table
Then Kernel comes up, but I could not see any successful trace logs for loading the IPU1 slave code.
Kernel logs are below:
<6>omap-iommu omap-iommu.4: mmu_ipu1 registered
<6>omap-iommu omap-iommu.5: mmu_ipu2 registered
<6>omap_rproc_init: skipping platform_device creation for ipu2
<6>platform omap-rproc.3: platform_device for rproc ipu1 created
<6> remoteproc0: ipu1 is available
<3> remoteproc0: failed to load dra7-ipu1-fw.xem4
Want to know where it has failed exactly. Is there any way to know from loaded xem4 is running or not? How to debug from here to find what goes wrong here?
Thanks,
Rabi