Hi,
I have updated to latest "TI RTOS v2.00.00.22 - TI RTOS for c2000" hoping it had the fix to the Ethernet problem on concerto control card discussed in my previous forum post http://e2e.ti.com/support/embedded/tirtos/f/355/t/329635.aspx. But the problem remains same and Ethernet module is not functioning as expected. The green LED on the Ethernet connector never comes ON and I can't establish any connection via Ethernet. We have already developed and completed software using TI RTOS, based on the TMDXCNCDH52C1 card (which is working fine) but this is now discontinued as the chip was changed to production version and upgraded to TMDSCNCDH52C1. TI RTOS Ethernet drivers do not seem to be working with this new board.
Would really appreciate if anybody can provide a solution to this problem as our whole project is on hold due to this issue.
Many Thanks,
Bin