Hello all,
(target C6678, sysbios 6.37.1.24, xdctools 3.25.5.94, ccsv6 6.0.0.00098)
At runtime here's what I do :
Plug SystInt 112, 113, 114, 115 to HostInt 32, 43, 54, 65 through CIC0
Plug SystInt 116, 117, 118, 119 to HostInt 32, 43, 54, 65 through CIC1
then when I open CpIntc ROV view I see :
As you can see for SystInt 116, 117, 118, 119 the Host Int is 0 instead of 32, 43, 54, 65.
I've step through my code and didn't see any error.
I'm wondering if it's not a bug in CpIntc ROV view because these interrupts are plugged through CIC1
I'll try to reproduce the issue in a simple SYSBIOS project.
Thank you,
Clement