We are porting over our application from using lwip to NDK. Here is our current configuration where we are using the USE_CPSW_DRIVER define :
Processor AM3352
Code Composer Version: 5.5.0.00077
Compiler TI v5.1.6
SYS/BIOS 6.35.4.50
NDK 2.23.2.03
XDCTools 3.25.1.65
These versions are compatible according to the Industrial SDK 1.1.0.4:
http://processors.wiki.ti.com/index.php/AM335x_SYSBIOS_Industrial_SDK_01.01.00.04_User_Guide
We get the following warnings when compiling eip_main.c, eip_ndk.c and hal.c:
'Building file: ../eip_main.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/bin/armcl" -mv7A8 --code_state=32 --float_support=VFPv3 --abi=eabi -me --include_path="C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include" --include_path="C:/Users/jc/workspace_v5_5/PST_sysbios/AIRtrac" --include_path="C:/Users/jc/workspace_v5_5/PST_sysbios/SPI_driver" --include_path="C:/Users/jc/workspace_v5_5/PST_sysbios/NAND_driver" --include_path="C:/ti/ndk_2_23_02_03/packages" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/protocols/ethernetip_adapter/firmware" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/protocols/ethernetip_adapter/drivers" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/protocols/ethernetip_adapter/include" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/os_drivers/include" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/os_drivers/include/CPSW" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/os_drivers/include/ICSS" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/starterware" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/starterware/include" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/starterware/include/hw" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/starterware/include/armv7a" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/starterware/include/armv7a/am335x" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/platform/am335x/include" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.0.0.8/sdk/starterware/nandlib/include" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.0.0.8/sdk/starterware/usblib/include" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.0.0.8/sdk/starterware/usblib/host" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.0.0.8/sdk/starterware/third_party/fatfs/src" --include_path="C:/ti/am335x_sysbios_ind_sdk_1.0.0.8/sdk/starterware/mmcsdlib/include" --include_path="C:/ti/AM335X_StarterWare_02_00_00_07/grlib/include" --include_path="C:/ti/AM335X_StarterWare_02_00_00_07/grlib/fonts" -g --gcc --define=am3359 --define=sys_bios_ind_sdk --define=idk_AM335x --define=evmAM335x --define=am335x --define=USE_CPSW_DRIVER --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="eip_main.pp" --cmd_file="./configPkg/compiler.opt" "../eip_main.c"
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 50: warning #48-D: incompatible redefinition of macro "ENXIO" (declared at line 72 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 53: warning #48-D: incompatible redefinition of macro "EBADF" (declared at line 59 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 56: warning #48-D: incompatible redefinition of macro "ENOMEM" (declared at line 70 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 57: warning #48-D: incompatible redefinition of macro "EACCES" (declared at line 57 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 66: warning #48-D: incompatible redefinition of macro "EINVAL" (declared at line 64 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 68: warning #48-D: incompatible redefinition of macro "EMFILE" (declared at line 67 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 80: warning #48-D: incompatible redefinition of macro "EINPROGRESS" (declared at line 96 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 86: warning #48-D: incompatible redefinition of macro "EMSGSIZE" (declared at line 97 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:\ti\ndk_2_23_02_03\packages\ti\ndk\inc\serrno.h", line 108: warning #48-D: incompatible redefinition of macro "ETIMEDOUT" (declared at line 103 of "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6/include/errno.h")
"C:/ti/am335x_sysbios_ind_sdk_1.1.0.4/sdk/starterware/include/hw/hw_cm_dpll.h", line 84: warning #1557-D: white space between backslash and newline in line splice ignored
'Finished building: ../eip_main.c'
' '
The warnings seem to be related to the NDK and are only seen in eip_main.c, eip_ndk.c and hal.c which were added to the project to support NDK.
Have we missed something obvious?
Thanks,
John C.