Hi,
I create a simple ezDSP5535 DSP/BIOS project, but there is no HWI interrupt generated.
Here is the code. I expect the keys (SW1, SW2) can trigger a gpio interrupt, which post a SWI. Then SWI has a LOG_printf output.
I set a breakpoint inside gpioISR, but nothing occurs.
I have used EZDSP5535_GPIO_init() to initialize GPIO. Are there anything I forget?
Thanks,
3036.ezDSP5535_switch_BIOS.zip
Void swiFxn0(Void);
Void task(Arg id_arg); /* Function for tasks created with Config Tool */
/** Interrupt Service Routine */
//interrupt void sarISR(void);
void sarISR(void);
void gpioISR(void);
extern void EZDSP5535_GPIO_init();
/*
* ======== main ========
*/
Void main()
{/*
Bool flag = 1;
CSL_SarChSetup param;*/
EZDSP5535_GPIO_init();
HWI_enable();
// SWI_post(&SWI0);
LOG_printf(&trace,"Main done!\n");
}
void gpioISR(void)
{
SWI_post(&SWI0);
;
}
void sarISR(void)
{
;
}
/*
* ======== swiFxn0 ========
*/
Void swiFxn0(Void)
{
LOG_printf(&trace,"swiFxn0 posts SWI1\n");
// SWI_post(&SWI1);
LOG_printf(&trace,"SWI0 done!\n");
}