For my code that compile without DSP/BIOS 5.42, I would use a SECTIONS statement such as
.buffer : > DARAM, to put the .buffer into DARAM space, where the .buffer was defined by
a pragma statement in the source code.
But then when I enable DSP/BIOS 5.42, the linker gives an errors saying it doesn't know which
segment to put in.
Also, under the Configuration tool to edit the *.tcf file, I will like to change the name of VECT segment under the MEM manager, but it doesn't give me the option to Rename the segment. It also only allows me to specify the base address, but doesn't allow me to change the segment length.
Why?
"warning #10247-D: creating output section ".buffer" without a SECTIONS specification"