I'm using CCS v5.5 + DSP/BIOS v5.42 and I have it hooked up to
a TMS320C5505 eZdsp USB Stick.
The Show Build settings and Target Configurations both are set to
C5500 family, USBSTK5505, and the connection is
Texas Instruments XDS100v2 USB Emulator. I also had enabled the following in the *.tcf file:
bios.enableRealTimeAnalysis(prog);
bios.enableRtdx(prog);
bios.enableTskManager(prog);
When I connect to device and load a program to run, the debugger says running.
But then when I try to enable the RTA, I see the both the RTOS Analyzer Configuration and RTA options are greyed out.
Does anyone know how to access the RTA (Legacy) option with the DSP/BIOS feature on that USB Emulator?
Chris