Hi there,
I am trying to increase the CPU clock of my c6747 custom board from 300Mhz to 450Mhz, while keeping the clock rate of the remaining peripherals before the change, such as SPI remaining at 1Mhz.
All these settings are done upon power up, i.e. not dynamically.
Fyi the 1Mhz SPI setting is working fine at SYSCLK1 300Mhz and the crystal's frequency is 15Mhz.
However, after
1) adjusting the PLL multiplier from 20 to 30 to produce a SYSCLK1 of 450Mhz and
2) changing the .tcf file under System>GlobalSettings>DSP Speed In MHz (CLKOUT) to 450Mhz,
the Spi's output clock changes from 1Mhz to 1.5Mhz
I suspect that the DSP/BIOS is not correctly informed of the change in DSP clock rate, causing the SPI to output a wrong clock rate. This is observed from the 1.5 times increase in SYSCLK1 corresponding to the undesired 1.5 times increase in SPI clockrate.
Fyi im using DSP/BIOS 5.41.04.18, Code gen tool 6.1.13, CCS 3.3.
Welcome any comments or solution.