Hello TI,
This week I built up a project with sysbios+lwip on sitara am3359 custom board acccording to the example in sysbios ind sdk version 1.1.0.4. I tried to put the emac to run under DUAL MAC mode. But when I run this project both of the port can finish the auto-negotiation, But only port 1 can be able to get the IP address from my switch. Port 2 never get the IP address from the switch.
I also tried to connect two port to two different switch (which belong to two different network segments). ALso the same thing happen. Looks like the port 2 is not configure currectly in ALE table or switch module. Can any one give me some suggestion? Is the DUAL MAC mode usable in this version of ind sdk?
Thank you very much!!
By the way,my software is like this:
CCS version 5.5.00077
SYSBIOS version 6.35.4.50
IND SDK version 1.1.0.4