Hi,
I'm using DK-TM4C129X , CCS6, tirtos_tivac_2_00_02_36, and uia_2_00_00_28
I want to use loggerstreamer2 mode.
how can I log raw data in the buffer which i created for the logger ?
where can I find the APIs for logging in this mode ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm using DK-TM4C129X , CCS6, tirtos_tivac_2_00_02_36, and uia_2_00_00_28
I want to use loggerstreamer2 mode.
how can I log raw data in the buffer which i created for the logger ?
where can I find the APIs for logging in this mode ?
Thanks
Hi Mostafa,
You can find example usage for LoggerStreamer2 in the cdoc for UIA. The log data is written with Log APIs (eg, Log_write()). The examples in the cdoc use Log_iwriteUCn(), which are optimized for speed. The UC stands for unconditional, and there is no check for whether or not logging is enabled, thus saving time. (Using Log_iwrite() allows you to specify the logger instance.)
Best regards,
Janet