Hi Guys,
I have been using CCSv5 + Sys/Bios + UIA + XDCTools for quite a while. Now, I want to migrate to CCS v6. But I'm wondering how to install CCSv6 + the components mentioned above. There is no need to stay with my old Sys/Bios and UIA versions.
It figured out, that with CCSv6 there are at least four ways to get this setup installed. My main requirement is, that the setup must be reproducible with regards to version of the compiler, Sys/Bios, UIA and XDCTools.
- CCSv6 Offline Installer + TI RTOS from App Center
- CCSv6 Offline Installer + Standalone TI RTOS Installer [1]
- CCSv6 Offline Installer + Standalone Sys/Bios Installer + Standalone UIA Installer [3]
- Standalone all: compiler, Sys/Bios, UIA, XDCTools
I'm interested in the advantage and disadvantages of these four options. The reproducibility of the setup is needed to be able to deploy the tool chain (compiler, Sys/Bios, UIA, XDCTools) to my build servers. At the end, the toolchain of the developer workstations and build servers must be identical.
System infos:
OS: Ubuntu 12.04
Target: C6000 familiy, mainly C674x
[1] http://downloads.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/2_00_01_23/exports/tirtos_c6000_setuplinux_2_00_01_23.bin
[2] http://downloads.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/bios/sysbios/6_40_01_15/
[3] http://downloads.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/uia/