I'm trying to the following steps:
1) Setup and start the network via NDK (no issues here)
2) afterwards, have a process outside of the NDK to add a static entry via LLIAddStaticEntry().
However, when I make the call, the DSP seems to hang up / crash. I have tried adding the llEnter and llExit function calls too but that didn't change the behavior. It works if I call LLIAddStaticEntry from the NetworkOpen function in NC_NetStart. How can I modify the ARP table entries externally?
Thanks,
Raj