Hi Champs,
I'm using IPC v1.25.03.15 for C6657 and planning to upgrade it to IPC v3.23.00.01.
So, dose the latest IPC support C6657?
Thanks in advance for your cooperation.
Regards,
j-breeze
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Champs,
I'm using IPC v1.25.03.15 for C6657 and planning to upgrade it to IPC v3.23.00.01.
So, dose the latest IPC support C6657?
Thanks in advance for your cooperation.
Regards,
j-breeze
J-breeze,
This release supports the following devices (though examples are not provided for all):
TMS320C6472
TMS320C6474
TMS320C6670
TMS320C6678
OMAPL138
TCI6638K2K (Keystone II) - Linux on HOST, SYS/BIOS on C66 DSPs
OMAP543X - QNX on HOST, SYS/BIOS on DSP, SMP-BIOS on IPU
DRA7XX (Vayu)
SYS/BIOS on HOST, DSP(s), EVE(s), SMP-BIOS on IPU(s)
SYS/BIOS on HOST, DSP(s), EVE(s), IPU1-0, IPU1-1, SMP-BIOS on IPU2
QNX on HOST, SYS/BIOS on DSP1, SMP-BIOS on IPU2
OMAP-L138 - Linux on HOST, SYS/BIOS on DSP
Find the more details at IPC user guide and release notes.
J-breeze,
In addition that, go through the wiki pages, this will give you more detailed info.
http://processors.wiki.ti.com/index.php/Category:IPC
http://processors.wiki.ti.com/index.php/IPC_3.x
I believe that the IPC_3.x does not support for C6657 device, it can support some other keystone-I devices. Refer the release notes and download link,
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ipc/index.html
Hi Pubesh,
Thank you for your suppport. I found the related information below.
o TI EP Wiki : IPC 3.x Migration Guide
(http://processors.wiki.ti.com/index.php/IPC_3.x_Migration_Guide)
- Device Support
For devices running BIOS on all cores, IPC 3.x supports all the same devices
as IPC 1.x. The BIOS-side code is all the same.
So, I am going to check the migration of IPC v1.2x examples.
If you have any the migration information, please let me know.
Regards,
j-breeze
Hi Pudesh,
Thank you for your support and information.
I'd like to make sure about previous posts that you have marked as answered.
So, would you mean the wiki info below is not correct?
For devices running BIOS on all cores, IPC 3.x supports all the same devices
as IPC 1.x. The BIOS-side code is all the same.
Regards,
j-breeze
J-breeze,
I did not say the wiki pages incorrect, the information about the migration can find at this wiki.
I did not get any doc other than this wiki for migration, so that I shared this wiki only. You may known this wiki early.
I'm chiming in to clarify a couple of things.
IPC 3.x adds support for a few multicore devices in additional to certain HLOS support.
See: http://processors.wiki.ti.com/index.php/IPC_3.x
If you are on a device that was previously support by IPC 1.x, there is no reason to move to IPC 3.x. Though we haven't removed any functionality between 1.x and 3.x, IPC 3.x doesn't add any value as the source are mainly identical for previously supported devices.
I hope this helps clarify the confusion.
Hi Arnie, Hi Pubesh,
Thank you for your support.
I understand and I could migrate a IPC v1.24 example to IPC v3.23. The example is SHM benchmark in PDK.
Thanks a lot.
Regards,
j-breeze