hello there,
currently i'm working on a SYS/BIOS project with an OMAPL138 SOM M1 module from logic pd consisting of two .out files (one for arm and one for dsp core).
the two cores are communicating via messageQ with each other.
when loading the projects with XDS510 everything works fine.
but if i convert the projects with AISGENtool to a single bin file and flash it on the module, the code execution on ARM stucks within HeapBufMP_open function (the function does not return).
both cores are up and running (controlled via LED) and ipc_start functions (on arm and dsp) return without error. so waking up the dsp core from arm does work.
does anyone has a clue what can be wrong here?
thank you for your help
peter