I have a project running under TIRTOS with NDK_2_23_01_01 using PPP Client to talk to a 3G modem via serial.
This is all working fine but I wish to drop the PPP layer by doing an LCP disconnect so that I can do clean shut down of a PPP session.
The PPP library only has pppNew, pppFree, pppInput, pppTimer, pppTxIpPacket functions.
The status function tells me if the PPP has disconnected, I want to initiate the disconnection. Would appreciate being advised how this is done, or if it can be done?