Hi, I'm going through the Kernel Workshop labs using a TM4C1294XL launchpad instead of the TM4C123GH6PM.
Currently having some issues setting up the clock.
In the Lab05 example code (TM4C123GH6PM) they set the clock via:
//Set CPU Clock to 40MHz. 400MHz PLL/2 = 200 DIV 5 = 40MHz
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
In the non TIRTOS "hello world" example (TM4C1294XL) they use:
//
// Run from the PLL at 120 MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
Do they perform the exact same function? The datasheet that details Clocks and PLL doesn't really cover this..
Also, does the following error below affect me?
http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/p/330524/1156581.aspx#1156581
Thanks,
Stephen