Hi all.
I need same support on TivaC129 board and NDK configuration.
I'm developing an application that need to change the IP parameters Runtime (i.e. during running application), this is why the user can choose IP static or dinamic during its setup made with a GUI istance.
The question is: do I have to use the NDK without XGCONF? or can I use the XGCONG to setup an initial configuration and then change it Runtime?
I've downloaded the package "nsp_1_10_02_09" but the only example I've found is cfgdemo but it's not for TIVA.
Thanks in advance
Marco Crivellari