Hi TI,
I am currently using concerto board (F28M35H52C1) and TIRTOS to interface with GPS module (Sparkfun Venus). I can successfully read data and write to console by using the syntax below.
UART_read(uart, &input, 1);
UART_write(uart1, &input, 1);
At this stage, I would like to configure the GPS module by sending binary message to GPS module to change the updata frequency. Such as, if I would like to make the frequency to be 10Hz, the following decimal value has to be sent in binary mode to the module. I had tried to use UART_write again, but this is just for string values. Could anybody help with this issue to indicate me how to do it?
10Hz : 160 161 00 03 14 10 00 04 13 10
Thanks in advance!
Ben