MCU: TM4C1294NCPDT
TI-RTOS: v2.01.00.03
NDK: v2.23.01.01
CCS: v6.0.1.0040
Hello,
I am working on implementation of Embedded Web Server on Tiva C MCU following the guidelines provided in the ppt presentation in the link http://processors.wiki.ti.com/index.php/TI-RTOS_HTTP_Example . On page 44 of the ppt file, its mentioned that we need to add efs_stdio.c (supplied in the zip file) to the main C file in order to make the html file be read & directed from the SD card. But since the functions like efs_createfile, efs_destroyfile have already been defined in the file efs.c in the OS folder of the NDK package, the compiler is giving an error "#10056 symbol "efs_createfile" redefined: first defined in "./DL_main.obj"; redefined in "./myfiles/2642.efs_stdio.obj" DL_Tiva_20141105".
Please help on how I can resolve the issue. I have gone through the posts "http://e2e.ti.com/support/embedded/tirtos/f/355/t/292751.aspx?pi199400=1" & "http://e2e.ti.com/support/embedded/tirtos/f/355/p/295118/1030893.aspx#1030893", but it seems not to help in resolving the issue.
Screenshot of the error in CCS compiler have been attached with this post in a zip file.
Thanks
Regards
Soumyajit