Hello CCS experts
I am looking at migrating from CCS v5.2 to v6.
The device target is C6424, custom platform.
I've installed CCS v6 and also upgraded to
- bios_6_41_00_26
- uia_2_00_01_34
From what I've gathered, XDC is "core" only, without any targets or platform support.
Is there a place once can download these separately? Or point to them from other versions?
OR
Is it only acquired via installing the TI-RTOS bundle?
Thanks!