Hello!
I need an example for Telnet echo (NDK TI-RTOS) for EK_TM4C1294XL.
I use CCS 6.01, tirtos_tivac_2_01_00_03
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I found 2 threads which may help you out. The second thread is also referenced in the first one. There are lots of links in the first thread to different resources.
http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/p/352227/1236062.aspx
http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/358322.aspx
Judah
This examples not use Ti rtos with NDK GUI.
I run a example
http://processors.wiki.ti.com/index.php/TI-RTOS_HTTP_Example
It work fine. Now I need to add in this project telnet echo. I enable in GUI NDK telnet module, create instance "telnet0". It have 2 function: Servicereport and Callback. What i need do now? Add this functions in main.c? Create a task? Need examples.