Hi all
MCU: TM4C1294NCPDT
TI-RTOS: v2.01.00.36
NDK: v2.23.01.01
CCS: v6.0.1.0040
SYS/BIOS 6.4..02.27 GA Release Note
Hello,
In the udpEcho_TivaTM4C1294NCPDT example (TI-RTOS for TivaC), the IP address of the board is set in the .cfg configuration file as indicated in the below lines:
Ip.address = "192.168.1.2";
Ip.mask = "255.255.255.0";
Ip.gatewayIpAddr = "192.168.1.2";
But how can I change these properties during run time? In my application, I have to give control to the user who can set these parameters as he wants.
Thanks