Hi All,
I am new on DSPs and Code Composer Studio and as a start with I'm trying to build hello example on CCS v5.5 (Example Projects--> SYS/BIOS-->C6000-->C66xx Multicore DSP--> TMS320C6678-->Generic Examples-->Hello Example). Firstly the error was about "could not open source file ti/targets/select.h", I manually added include paths to the include options under the project properties and this problem was solved. After that I received 3 error, these are:
#10234-D unresolved symbols remain
#10010 errors encountered during linking; "hello_TMS320C6678.out" not built
#10008-D cannot find file "./configPkg/linker.cmd"
I am using TMS320C6678 EVM and a Blackhawk XDS560v2-USB Mezzazine Emulator. I think, I should add some paths to linker options or somewhere else but I don't know which path or where I should add? What do you suggest me more?
If you can help me about this, I will be very glad. Thanks in advance.
Duygu