I meet a problem when run the messageQ module.I use the MessageQ example in the IPC module as a reference.The difference is that I create two projects,that is different exectuable (*.out) files run on different cores.
in my project, core0 send message Q to core1.Some code is below:
the SharedRegion has been modified in the .cfg file.
core0 task:
{
·······························
HeapBufMP_Params_init(&heapBufParams);
heapBufParams.regionId = 0;
heapBufParams.name = HEAP_NAME;
heapBufParams.numBlocks = 1;
heapBufParams.blockSize = sizeof(MessageQ_MsgHeader);
heapHandle = HeapBufMP_create(&heapBufParams);
/* Register this heap with MessageQ */
MessageQ_registerHeap((IHeap_Handle)heapHandle, HEAPID);
·····················
}
core1 task:
{
··············
do
{
status = HeapBufMP_open(HEAP_NAME, &heapHandle);
} while (status < 0);
``````````````````
}
the problem is that core1 can't open the heap, I want to ask what should I notice before I call the HeapBufMP_open()?
Is there anything I should do to make sure the function runs properly?
Thank you very much!