MCU: TM4C1294NCPDT
TI-RTOS: v2.01.00.03
NDK: v2.23.01.01
CCS: v6.0.1.0040
Hello,
I have started with the TI-RTOS example fatsdusbcopy to evaluate file copy from SD card to USB Thumb Drive. After evaluating, I added Embedded Web Server into my project following httpServer example of Concerto Board (processors.wiki.ti.com/.../TI-RTOS_HTTP_Example).
After this, when I am trying to do the SD card to USB Thumb Drive copy, the task gets stuck when the function "USBMSCHFatFs_open" is called. During the development of the embedded web server, I was blocking this sdcard to usb copy task.
Can anyone suggest some way out?
Section of the code is shown here as provided in the example also:
// Mount and register the USB Drive
USBMSCHFatFs_Params_init(&usbmschfatfsParams);
usbmschfatfsParams.servicePriority = 3;
usbmschfatfsHandle = USBMSCHFatFs_open(Board_USBMSCHFatFs0,
USB_DRIVE_NUM,
&usbmschfatfsParams);
Thanks
Regards
Soumyajit