Hi,
We are running SYS/BIOS with NDK on our production board using the CPSW interface. Our current software versions:
Processor AM3352
Code Composer Version: 6.0.1.00040
Compiler TI v5.1.6
SYS/BIOS 6.40.3.39
XDCTools 3.30.3.47_core
NDK 2.24.0.11
We currently are running a fixed IP address with four TCP sockets being created and serviced. The PC application uses the four sockets for different data and there is also a command window running a 'ping' command on the PC. The pings are 1418 bytes in size and have a good response for awhile until it hits some type of issue. The ping response times will increase from <1msec to approx 40msec and then miss a single ping before returning to a ping response of under <1msec. This anomaly happens regardless of whether the PC application is connected or not. If we run a default ping size of 32bytes this issue does not happen. Is there NDK debug information or configuration that could help pinpoint what is going on?
Thanks,
John C.
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=47ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=46ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=44ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=43ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=42ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=41ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=39ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=37ms TTL=255
Reply from 10.1.9.200: bytes=1418 time=36ms TTL=255
Request timed out.
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255
Reply from 10.1.9.200: bytes=1418 time<1ms TTL=255