Hi,
Development environment:
ccs 6.0.1.00040
tirtos_tivac_2_00_02_36
TivaWare_C_Series-2.1.0.12573
I am looking at tm4c to find a similar function like "UARTprintf()" that displays debugging messages on "putty" .
In uartlogging example, I expect "Log_print2" outputs to "System analyzer", also display something on the terminal (Putty).
However I don't see anything in "System Analyzer" but displaying broken characters on "putty".
Baud rate:9600
data bits : 8
stop bits :1
parity: None
flow control : None
What do I have to do to be able to see messages on Putty?
Is "LoggerIdle" the only way to display messages on the "putty" simultaneously with displaying on ccs console or system analyzer?
Thanks,
Jin