Hi,
I am using CCS V6 for a TIVA tm4c129encpdt processor.
What is the proper way (if any) to conditionally include or exclude NDK for a TI-RTOS project with a separate build configuration?
I have a project that can be compiled with several different build configurations depending on variations in functionality. Now I need to add a new build configuration for a new model that is going to communicate with a device with Modbus RTU over TCP and therefore I need to add the NDK. But I would only like to add it for just that build configuration. Is that possible? Can I use predefined symbols to conditionally include modules in app.cfg or perhaps have several app.cfg which can be set to be excluded from build so that different configurations uses different app.cfg?
Or do I need to include NDK for all configurations or make a new project and link the files from the other project into that?
/Ruben