Hello,
one of my customers is facing issues on his Windows 7 system when using the cygwin1.dll version 1.5.25, which is part of our current (and older) XDCtools deliveries. He thinks that this old version of cygwin1.dll does not play well on his system, especially together with Symantec Endpoint Protection.
The issue that he was facing is about some "permission denied" error. It seems that configuro is using the cygwin cp command to generate new linker.cmd files, but makes it read-only. Following writes (to modify) the linker.cmd files will fail with a permission denied then.
He was able to solve his issue be replacing the cygwin1.dll with a new version (1.7.33) from the cygwin.org site.
Would it make sense to upgrade cygwin1.dll that comes with the XDCtools to a newer version?