When I build my project in CCS v5.5.0 imported from CCS v3.3, I get these errors and I can't open my .tcf file with teh Tconf editor:
**** Build of configuration Debug for project SingenX05-3a ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../SingenX05-3.tcf'
'Invoking: TConf'
"C:/ti/bios_5_42_01_09/xdctools/tconf" -b -Dconfig.importPath="C:/ti/bios_5_42_01_09/packages;C:/CCStudio_v3.1/DSP-BIOS_5.20.05.34/packages;" "../SingenX05-3.tcf"
js: Reference constraint violation: H0SARAM is an illegal value for MEM.LOADSTUBMEMSEG
gmake: *** [SingenX05-3cfg.cmd] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
When I try to open the .tcf file with the DSP/BIOS Configuration tool, I get the following:
js: Reference constraint violation: H0SARAM is an illegal value for MEM.LOADSTUBMEMSEG
Correct any script errors in C:/CCS_Workspace_v5_5/.metadata/.plugins/org.eclipse.rtsc.xdctools.buildDefinitions.DSPBIOS/.gconf/SingenX05-3a/SingenX05-3a/SingenX05-3.tcf
using the Configuration Tool or a text editor, if necessary.
TConf initialization arguments:
-e environment['config.importPath']='C:/CCS_Workspace_v5_5/SingenX05-3a;C:/ti/bios_5_42_01_09/packages;C:/CCStudio_v3.1/DSP-BIOS_5.20.05.34/packages' -e environment['config.scriptName']='SingenX05-3.tcf'
__________________________________________________
How can I correct script errors when I can't even open the configuration tool?
I'm lost. Please help. Please note that this project builds fine in CCS v3.3, but it's on a Win XP laptop and I can't use that for development anymore. I need to use my win 7 PC with CCS 5.5.0 and eventually on CCS v6. The only reason I'm not using CCS v6 now is that my emulator, Signum JTAGJET-C2000, doesn't have the driver files ready yet for CCS v6, but they say they will in the next few weeks.
I've spend a few weeks trying to understand these error messages and fix this, but I'm lost. I was OK on CCS v3.3, but the CCS v5.5.0 tools seem harder to figure out, especially with regard to TCONF and DSP/BIOS. Note that my project somewhere is making a reference to DSP-BIOS_5.20.05.34/packages, but I can't figure out how to find out where in my project this is coming from so I can change it to a DSP/BIOS version that I have installed, like DSP/BIOSv 5.42.1.09.
Thanks for your help. An expedited reply would be greatly appreciated. Once I get past this initial inability to get my old project building in CCS 5.5.0, I'll be OK for new projects.