Hi,
Does anyone whats the minimum footprint that the TI RTOS would need?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does anyone whats the minimum footprint that the TI RTOS would need?
This is for the TIVA C series...specifically for TM4C129X
Memory required: Flash and ROM
Regards,
Rashmi
Rashmi,
Do you have TI-RTOS for TivaC installed? You can download it here. We have an example for the TM4C1294XL, the Empty (Minimal) project that gives a realistic benchmark of the footprint. It has a basic task and no heap. You can import the example and evaluate it further.
Let me know if it helps
Moses
Hi Moses,
I imported the minimal example project
Flash size: 22366 bytes
SRAM: 8672 bytes
So, can I consider this as memory needed just for the RTOS itself?Since this has minimal tasks
Regards,
Rashmi