i have use tibios pakage; when i use
void
CANIntRegister(uint32_t ui32Base, void (*pfnHandler)(void))
this function ,error occur, the error is :
.vtable section locate in sram 0x20000000; .vect section also locate in sram 0x20000000;
.vatable is the section defined in interrupt.c in standard driverlib;
.vect is defined by tibios auto configure;
how can i do ,