I recently acquired a sensortag reference CC2650SensorTag rev 1.2, I am trying to connect it to an accelerometer (an external one not the one included) via SPI, I opened a project using the TIRTOS for simplelink add on on the CCS (see picture)
when I open Board.h this is the pin definition I get for the SPI0CLK
but when I open the sensortag example from the BLE stack the pin definition looks like this..
why do they have a different SPI0_CLK? which one is the correct one ? or is it something I have to change in the configuration?