Hi, guys.
I'm studying SYS/BIOS with MY EVM6678.
As you know, TI offers many example codes for students like me.. :)
For I'm using C6678 multicore processor, I have to use an operating system to support it.
I think SYS/BIOS is better than Linux in my case.
SYS/BIOS has HAL(Hardware Abstraction Layer) and it is convenient.
But sometimes I should use CSL(Chip Support Library) or PDK(platform development kit) which I think access hardware directly.
So I think it is sometimes dangerous to use both at the same time. I mean, in the same project.
Can I use them at the same time? isn't it dangerous?
If so, is there some good strategies to avoid the problem?
James