Hi Guys,
I want to use the am3359 ice v2 board to transfer data through ethernet/ip protocol and get the command from upper level app also through ethernet/ip protocol. Now all the low level code has been finished(such as ADC sample, digital input/output and so on) and now it's time to transfer the data. But it seems I totally lost these days(I am a new man in the ethernet/ip communication field). Can anyone give me some suggestions, any documentation or any application notes? Can anyone point me to the right direction?
For example, I added the ADC sample code into the ethernerip_adapter example code and want to send the measured data from ADC through ethernet/ip protocol. How can i modify the ethernetip_adapter code so that I can send the data through the ethernet/ip protocol?
I am very appreciate your help and thank you so much!
Regards,
Aaron