Hello everyone,
(ccsv6, target C6678, sysbios 6.41.01.36, xdctools 3.30.05.60, uia 2.00.02.39)
The aim of LoggerSM is to write execution logs in shared memory.
These logs have a timestamp associated to them. (optional)
The aim of XDC Timestamp proxy is to provide a single way to timestamp events accross the system.
In theory, once set, all sysbios/IPC/UIA modules use it to timestamp events
However, and this is the problem I'm reporting, it's not the case for the LoggerSM module for C64p family of targets (C6678 included).
Behaviour for C64p family: TSCL and TSCH is used to timestamp logs (as you can see in LoggerSM.c runtime side)
Expected behaviour: always use Timestamp_get64() which calls the Timestamp proxy.
In the meantime I've patched my UIA package to fix this.
I hope it gets resolved in the future.
Regards,
Clement