Hello everyone,
(target C6678, CCSv6, UIA 2.00.2.39)
The UIA LoggingSetup module has several configuration settings
One of them is:
LoggingSetup.loggerType
which offers the choice
LoggerType_MIN ; STOPMODE (value by default) ; JTAGRUNMODE ; RUNMODE ; IDLE ; STREAMER2
LoggerSM is NOT in this list and should be.
LoggerSM is meant to be used along LoggingSetup
As a result a STOPMODE logger instance is present in the final application (along with the LoggerSM instance)
Will this be fixed ?
Regards,
Clement