Hi everybody,
I have a problem with my UDP communication.
Compiler failure message:
network_api.c:160:83: warning: pointer targets in passing argument 2 of 'recvfrom' differ in signedness [-Wpointer-sign] actDataSize = recvfrom(pObj->clientSocketId, dataBuf, tmpDataSize, 0, (struct sockaddr*)&pObj->addr, &sendsize);
In file included from c:/VISION_SDK_02_06_00_00/vision_sdk/tools/network_tools/build/../common/inc/network_api.h:7:0, from network_api.c:2: c:\vision_sdk_02_06_00_00\ti_components\cg_tools\windows\codeblocks\mingw\include\winsock2.h:548:32: note: expected 'char *' but argument is of type 'UInt8 *'WINSOCK_API_LINKAGE int PASCAL recvfrom(SOCKET,char*,int,int,struct sockaddr*,int*);
Function:
int Network_read(Network_SockObj *pObj, UInt8 *dataBuf, UInt32 *dataSize) { int actDataSize = 0; UInt32 tmpDataSize; int sendsize = sizeof(pObj->addr); tmpDataSize = *dataSize; while(tmpDataSize > 0) { actDataSize = recvfrom(pObj->clientSocketId, dataBuf, tmpDataSize, 0, (struct sockaddr*)&pObj->addr, &sendsize); if(actDataSize<=0) { *dataSize = 0; return -1; } dataBuf += actDataSize; tmpDataSize -= actDataSize; } return 0; }
Struct:
typedef struct { SOCKET clientSocketId; UInt32 serverPort; char ipAddr[32]; SOCKADDR_IN addr; UInt32 protocol; } Network_SockObj;