Hi,
We are using Tiva TM4C129xNCZAD in one of our custom boards running sys/bios (v6.40.1.15). Tiva controller is getting stuck during boot some times when board is power on. Connecting to CCS using JTAG at this stage shows below stack status. Some times function call sequence will be slightly different on error but ti_sysbios_family_arm_lm4_Timer_masterEnable__I will be involved in every errors case. Are there any know issues which can cause failure of this function?
abort() at exit.c:117 0x000110CE
exit(int)() at exit.c:108 0x000110F8
xdc_runtime_System_exit_E(int)() at System.c:86 0x000126E8
ti_sysbios_BIOS_exitFunc_I(int)() at app_pem4f/c:2,984 0x0001271c
ti_sysbios_family_arm_m3_Hwi_excHandlerMax__I(unsigned int *, unsigned int)() at Hwi.c:920 0x0000C3E8
ti_sysbios_family_arm_m3_Hwi_excHandler__I(unsigned int *, unsigned int)() at Hwi.c:812 0x00012340
ti_sysbios_family_arm_lm4_Timer_masterEnable__I() [tiva_test.out] at 0xFFFFFFF8
abort() at exit.c:117 0x000110CF
0x0000000C (no symbols are defined for 0x0000000C)
- Pratap.