I’m working on an application which requires the following NDK library:
os.aa15fg
Currently, I’ve manually updated the application configuration by including “os.aa15fg” in the list of libraries and also a library search path to this library via CCS.
In my project cfg file, I’m using other NDK libraries as follows:
var Global = xdc.useModule('ti.ndk.config.Global');
var Ip = xdc.useModule('ti.ndk.config.Ip');
var Tcp = xdc.useModule('ti.ndk.config.Tcp');
var Udp = xdc.useModule('ti.ndk.config.Udp');
var Telnet = xdc.useModule('ti.ndk.config.Telnet');
Each of the above xdc.useModule cause a library to be linked. However, I don’t see means of xdc to link in the os.aa15fg library because package.xs file of “os”, the getLibs is basically blank.
How was it intended for a user to link in os.aa15fg via xdc?