Hi.
(I asked this question in a different thread, but didn't get an answer)
I have a TIVA device, which supports 1 Mbps rate on I2C bus, but TI-RTOS I2C driver only supports 400 Kbps.
Is it possible to use the driver with FM+ mode? If so, how is it done?
And another question (also asked in a different thread):
I have 2 tasks with same priority, each using different I2C channel in blocking mode.
Task #1 calls I2C_Transfer and blocks.
What happens when task #2 calls I2C_Transfer immediately after task #1 ? Does it wait for task #1 to complete the transfer, or these two calls are run simultaneously, because 2 different I2C channels are used?
Thanks.