Hello!
I'm trying to implement UartEcho example on our custom PCB boards that has 5X5 CC2650. But was unable to do so. Here are the list of modifications I've done to the sample project.
1. Included "ti/drivers/pin/PINcc26XX.h" and "ti/drivers/uart/UARTCC26XX.h" in uartecho_cc26XX.c
2. Defined CC2650EM_5XD in Properties -> Build -> ARM Compiler -> Advanced Options -> Predefined Symbols
3. In Board.h, I commented #define CC2650EM_7ID and defined CC2650EM_5XD. But I'm getting this error:
Cortex_M3_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.0)
Kindly help me solve this problem.
Thanks
Teja