This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 and CC3100

Other Parts Discussed in Thread: CC2640, CC3100

Hi,


I have a board that has connected the CC3100 to a CC2640 via SPI and I am trying to compile the driver from ti\tirtos_simplelink_2_13_00_06\packages\ti\drivers\wifi\cc3100 with IAR Embedded Workbench.

I am getting these errors:

Warning[Pe223]: function "GPIOIntDisable" declared implicitly C:\ti\tirtos_simplelink_2_13_00_06\packages\ti\drivers\wifi\WiFiCC3100.c 116
Error[Pe140]: too many arguments in function call C:\ti\tirtos_simplelink_2_13_00_06\packages\ti\drivers\wifi\WiFiCC3100.c 465

The code calls GPIOPinWrite(hwAttrs->enPort, hwAttrs->enPin, hwAttrs->enPin);
But GPIOPinWrite from gio.h is defined like this: void GPIOPinWrite(uint32_t ui32Pins, uint32_t ui32Val)

So I am doing something wrong here. Is there a example for CC2640+CC3100 that I missed? Or documentation how to do it?

Thanks

Sebastian