Hello
We are making a TM4C129xNCZAD microcontroller based custom board.
We are interfacing a 480x272 LCD in raster board (we are at present using only 4 bpp, so we are setting aside 64K of SRAM for framebuffer) and RFID reader(MAXIM Reader IC) is interfaced over SSI2. I am using separate GPIO pin for CS.
We are facing a weird problem explained below
When LCD is enabled
The application to read/write to the RFID tag is able to detect the tag. All further operation of selecting Tag, Reset the Tag, Read/Write to the Tag fails.
The moment LCD is disabled
The same application is able to detect tag, select Tag, Reset the Tag, Read/Write to the Tag
I will be uploading the relevant parts of the code (after removing some code that is under NDA ) tomorrow.
Is there any conflicts between SSI2 and LCD controller on TM4c129XNCZAD
Platform:
TI-RTOS 2.14
ARM Compiler 5.2.5
Controller: TM4C129XNCZAD
Thanks in Advance
Narendra